DUG_Connected Thermostat 16 A, ZB_WH-06

Creating a Moment

A Moment allows you to change the state of multiple devices with a single tap. Moments act like scenes, allowing you to control several devices all at the same time.
  1. On the Home screen, tap .
  2. Go to Moments > to create a moment.
  3. Enter the name of the moment (A).
    TIP: You can choose the cover image that best represents your moment by tapping .
  4. Tap Add actions (B) to select the list of devices.
  5. In the Select devices menu, you can select the devices (C).
  6. Once all the devices are selected, tap Done.
  7. On the Moment creator page, select the device to set the condition. For example, select heating.
    • Set the required temperature using the slider (D).
      NOTE: If you move the slider to the bottom of the bar, Frost Protection mode is activated. In this mode, the system maintains the room temperature at 5 °C.

    When the desired condition is set, tap Set.

  8. Once all conditions are set, tap Save.
Once the moment is saved, it is visible on the Moments tab. You can tap on the moment to enable it.
TIP:
  • If you want to see the created moments on the Home screen, go to Home > > Home screen > Moments. Enable the toggle button to view moments on the Home screen.

  • You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.