DUG_Push-button Module, 1-gang/2-gang_WH-09

Resetting the Device in Quick Home Connect

It is necessary to reset the devices in the following scenarios:

When reset is done successfully. The Wireless switch and device returns to factory default.

  • Integrating into Wiser System

    • If you wish to integrate the devices into Wiser System, reset all the devices in Quick Home Connect and refer to pairing the device with Wiser Hub/Gateway.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.