DUG_Push-button Module, 1-gang/2-gang_WH-09

Pairing the device with the Wiser Hub

You can pair your Push-button module (mounted on the insert) with the Wiser Hub to access and control the insert behind it.
  1. On the Home screen, tap .
  2. Tap Devices > > Lights / Shutters > 1-gang.
    TIP: You can also navigate by tapping Control > > Lights / Shutters > 1-gang.
    NOTE:
    • 1-gang Push-button module for switch, dimmer and shutter.

    • 2-gang Push-button module for switch and dimmer.

  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    IMPORTANT:
    • The QR code is located on the back side of the push-button module and is not visible when it is installed on the insert. Refer to the installation instructions for removal and reinstallation.

    • If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the MAC Address and Install Code, then tap Connect. The app will verify if the MAC address and Install code are valid.

    • (B): Tap this option if you are unable to find the MAC address and Install code.

  4. Tap Next, then short press the top-center of the 1-gang Push-button module 3 times and make sure that the LED blinks amber
    TIP: In case of 2-gang Push-button module, short press the top-right Push-button module 3 times.

    Wait for a few seconds until the LED turns green and the app confirms that the device is joined.

    NOTE: If the LED is blinking green and red, see the instructions by tapping LED blinking green and red? or refer to the Troubleshooting topic.
  5. Tap , enter a name of the device (example, switch, dimmer, shutter) tap Next and assign the device to a new room or an existing room.
    • If you have assigned the name as switch or dimmer, tap Next. Once the pairing process is completed, the device name is listed on the Control tab under the All and Room tabs.
    • If you have assigned the name as shutter, proceed from step 6 to step 10.
  6. Tap Next > and select a Device Type:
    If you have selected the device type as:
    • Shutter: Proceed to step 7.
    • Shutter with tilting slats: Proceed to step 8 and step 10.
  7. Tap Shutter > Next and enter the open/close duration of shutter. Refer to Setting default run time.
  8. Tap Shutter with tilting slats > Slat Type, select a slat type and tap Set:
    • Horizontal
    • Tilted
    • Vertical
  9. Tap Next and enter the following durations:
    1. Open duration: Time taken to open the shutter.
    2. Close duration: Time taken to close the shutter.
    3. Tilt duration: Time taken to rotate the slats completely from closed to open position.
  10. Tap Submit.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    The push-button module is now listed on the Control tab under the All and Room tabs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.