DUG_Push-button Module, 1-gang/2-gang_WH-09

Switch

Using the Wiser Home app, you can rename the 1-gang switch, edit or assign a new location, identify, and delete the 1-gang switch from the system.
NOTE: Configuring the device shown is for a 1-gang switch, and the same can be done for a 2-gang switch.
  1. On the Home screen, tap .
  2. Tap Devices > Lights > 1-gang to locate to the Device Details screen.

    A

    Device Name: Tap to change the name of the device.

    B

    Location: Tap to assign the Device to any room (such as living room, bedroom, kitchen etc). Refer to Setting the device location for more details on how to set the location.

    C

    LED Indicator Behaviour: Tap to set the LED indicator behaviour of the device as per your preference. Refer to Setting up the LED Indicator Behaviour for detailed information on each options.

    D

    Identify: Tap to identify the device.

    NOTE:
    • This feature flashes the 1-gang switch LED, so you can identify the actual device. It also switches connected loads on/off.

    • The 1-gang switch LED will continue to flash until you tap OK.

    E

    Delete: Tap to remove the device from the system.

    F

    Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device.

    • Good Signal (between 0 & -54dBm)

    • Normal Signal (between -54 & -79dBm)

    • Poor Signal (<-79dBm)

    • No Signal (device is offline)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.