DUG_Push-button Module, 1-gang/2-gang_WH-09

Resetting the device

You can reset the push button to the factory default. It can be reset manually at any time, e.g., when the Hub is replaced.

Short press the top-center push button 3 times and hold for 10 seconds to reset the device to the factory default mode.

TIP: In case of the 2-gang push button, short press the top-right push button 3 times and hold for 10 seconds to reset the device to the factory default mode.
NOTE: All configuration data, user data and network data are deleted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.