DUG_Push-button Module, 1-gang/2-gang_WH-09

Setting the configure duration

Each shutter motor varies in the time it takes to complete the opening/closing movement (i.e., edge to edge). Therefore, the opening/closing time of the shutter must be determined in the app.
To determine the configured duration, manually open/close the shutter.
  1. Record the time it takes to open/close the shutter completely.

  2. Record the time it takes to rotate the slats completely from closed to open position for shutter with tilting slats.


Follow the procedure according to your shutter type:
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.