DUG_Unica SSO_WH-10

Creating an automation

  1. On the Home screen, tap .
  2. Go to Automation and then tap to create an automation.
  3. Enter the name of the automation (A) and select any of the following conditions to trigger an automation.
    • All conditions: All conditions must be met to trigger an automation.

    • Any condition: Any one of the condition must be met to trigger an automation.

    TIP: You can choose the cover image that represents your automation by tapping .
  4. Tap Add conditions (B) and select any of the following (C).
    • Device status change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor.
    • Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more information about Away Mode, refer to the system user guide.
    NOTE: Maximum 10 conditions can be added.
  5. To start your automation at a particular time, tap When > Add time and select any of the following (D):
    NOTE: Maximum 10 time entries can be added.
    • Specific time of day - The automation will trigger at a specific time of the day, such as at sunrise, sunset, or at 8:00 AM.
    • Period of time - The automation will be trigger during time periods such as from sunrise to sunset, or sunset to sunrise, or from 8:00 AM to 5:00 PM.
    1. In this example, we will choose Specific time of day and then select Sunset as the start time for the automation.
    2. After choosing the automation start time, tap on Set on the upper right corner.
  6. To add an action, tap Then > Add an action and select any of the following (E):
    NOTE: Maximum 10 actions can be added.
    • Control a device - Select the device and set the desired state of the device.
    • Send notification - You will be notified if the condition is met.
    • Activate a moment - Select a Moment to activate during the automation.
    • Wait - This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.
    1. In this example, we will initially select Control a device and select Smart Socket (F) as the device to trigger an action, later, we will select for the Wait option to add a delay in the automation.
      IMPORTANT: You cannot select the same device that you selected for Add conditions in Step 4. The device should be different.
    2. Set the state, such as On/Off state of the Smart Socket. Then, tap Set located on the upper right corner.
    3. Again, tap Add an action and select Wait option.
    4. Scroll through the minutes and set the wait time to 1 minute. Then, tap Set located on the upper right corner.
  7. Tap Save.
    The saved Automation is displayed on the Automation page. Tap the toggle switch (G) on the Automation page to enable/disable the Automation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.