DUG_Unica PB Dimmer_WH-08

Editing a schedule

  1. On the Home screen, tap Automations > Schedules.
  2. Tap the schedule you want to edit.
  3. Tap the SCHEDULE DETAILS and you can do the following actions:
    • Rename the schedule (A).
    • Within the Applies to (B) menu, you have the option to select from the listed devices or deselect those that are already selected.
    NOTE: When the above changes are edited, the schedule is saved automatically.
  4. Under the EVENTS (C) menu, you can do the following actions:
    • Tap to update an event, such as STATE (lights Off or dimming level in %), WHEN (sunrise/sunset or a specific time range), and you can also delete an event.
    • Tap Set to save the schedule.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.