DUG_PowerTag-E_WH-11

Checking device consumption

Using the Wiser Home app, you can monitor the live, history of Grid, Solar and individual loads as well as statistical analysis of energy consumption of all the loads installed with PowerTag.
  • Live: Provides live data of the grid consumption and live status of where the power is coming from:

    • Grid to Home: Import

      (Home consuming power from Grid)
    • Home to Grid: Export (Excess power from Solar production fed to Grid)

    IMPORTANT: It is necessary to install PowerTag on Grid and additional power sources such as Solar, Solar and Battery to have accurate data of powerflow.

  • History: Provides history of power consumed by loads. If there is an existing On Grid solar system, the app provides history of imported and exported energy.

  • Insights: Provides information on energy savings and annual bill for the tariff set.

  • History and Insights for Personalized Energy Insights: Provides estimated energy breakdown of your home’s consumption. Energy comparison with similar homes and top energy saving tips.

    NOTE:
    • Live data is not shown.

    • History is only shown for months and years.

    • All energy insights are not shown at the same time.
      Example: A breakdown of energy for the previous month is available on the first day of the month.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.