DUG_PowerTag-E_WH-11

Pairing the main device

To pair the main device:
  1. On the Home screen, tap  .
  2. Tap Devices >  >  Energy.
  3. Select PowerTag Energy (A).
    TIP: You can also navigate by tapping Control > > Energy > PowerTag Energy.
    NOTE: Only the Energy tab is available to users in the Nordics and Belgium.
  4. The Device Discovery page will search for a minute to display the available PowerTags.
  5. If there is more than one PowerTag is available, select one among them (B).
  6. On the Device Configuration page, tap Identify to recognize the main PowerTag. This will be the Grid PowerTag measuring the main incomer.
    A notification window is prompted and the status LED flashes fast in green on the PowerTag.

  7. Tap OK on the notification window when you have finished identifying the PowerTag.
  8. Tap (C) to assign a label to the main PowerTag.
    The label list appears on the Type page.
  9. Select a label type (D) and tap Save (E).
    NOTE: It is recommended to select Gridas a label to represent the main PowerTag.
    Once the Grid type is selected, by default the Name is assigned as Main Incomer.
  10. Tap (F) and select Yes/No if you have solar panels installed.
    The power direction will be enabled automatically (H).
  11. Set the Grid Limit (G).
    NOTE: Grid limit is the maximum permissible power on the Grid on your contract. It will help to prevent power tripping by shutting down loads in order to keep the power consumption under a defined limit. By default, the grid limit is set to measure in kVA.

    Select your grid limit (kVA/A/kW) from the dropdown menu, then tap and enter a value using the dial pad as per your country. The following table displays the default values within the range:

    Country

    Default Value

    Range

    France

    36 kVA

    1–42 kVA

    Germany

    60 A

    15–160 A

    Spain

    15 kW

    1–42 kW

    Belgium

    40 A

    15–160 A

    Sweden

    20 A

    16–63 A

    Finland

    20 A

    16–63 A

    Denmark

    25 A

    25–35 A

    IMPORTANT: You cannot enter a value that is greater or less than the specified range.
  12. Enable the Reverse Direction toggle switch (I), if the power direction is from Home to Grid.
    IMPORTANT: Enabling Reverse Direction ensures the power direction is correct.
  13. Tap Save (J).

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    Now, you can see the newly added device on the Control tab under the All and Room tabs.


    NOTE: If you only have single PowerTag in the entire Wiser System, the Control page will not be visible. All functions will be accessible through the Home page.
    NOTE: You will be notified to enter the tariff after the PowerTag is commissioned, refer to Setting Tariff
    NOTE: If you have already configured your tariff, you will be directed to Home screen to view the status of device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.