DUG_System M and System D - Wireless Switch_WH-08

Resetting the device

You can reset the Wireless switch to factory default manually under the following conditions:

To reset the Wireless switch:

  1. Short press the top-right push button three times (< 0.5 s) and then press and hold the push button (>10 s).
    TIP: In case of the 1-gang Wireless switch, short-press the top-center push button three times (< 0.5 s) and then press and hold the push button (>10 s).
  2. After 10 s, the LED starts blinking red, then release the push button.
    The LED stops blinking upon successful reset of the device.
  3. The Wireless switch restarts and blinks green for a few seconds.
    NOTE:
    • After reset, the LED turns Off to save the battery.
    • All configuration data, user data, and network data are deleted.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.