DUG_Wiser 16A Relay for Temperature Control_WH-08

Identifying the device

Using the Wiser Home app, you can identify the Relay from the other available devices in the room.
To identify the Relay:
  1. On the Home screen, tap .
  2. Tap Devices > 16A Relay > Identify (A) to rename the Relay.
    NOTE:
    • This feature flashes the Relay LED, so you can identify the actual device.

    • The Relay LED will continue to flash until you tap OK.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.