DUG_Wiser 16A Relay for Temperature Control_WH-08

LED indications

Normal use

Status

User Interaction

Description

Power on

Flashing orange

In connection with the Wifi gateway

 

Off: heating off Steady

green: heating on

Pairing in progress

Alternating orange and green flashing

Not paired

Off: heating off

Steady orange: heating on

Degraded mode
(no connection with the thermostat or with the hub)

Flashing red: heating off

Steady red: heating on

Manual Test / Forcing

Flashing green: heating on due to forcing

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.