Pairing the device with the Wiser hub
- On the Home screen, tap
.
- Tap and tap Climate > .
- Tap Scan QR code and allow the Wiser
Home app to access your camera. Then, scan the QR code located on
the device.IMPORTANT:
-
The QR code is located on the device and is not visible when the device is installed on the wall. Refer to the installation instructions for removal and reinstallation of the device.
- If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.
If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:
-
(A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI-64 and Install code are valid.
-
(B): Tap this option if you are unable to find the Mac Address/EUI-64 and Install code.
-
- Once the device is validated, tap Next, press the Set button until the LED flashes green/amber.
- On the 16A Relay Setup page, select the control type Relay or Pilot wire.
- Tap Next to enter the relay name and assign it to new room or an existing room and tap Submit.