DUG_Wiser 16A Relay for Temperature Control_WH-08

Troubleshooting

Symptom

Possible cause

Solution

The relay displays offline in the app or the LED flashing or solid red.

  1. Weak or no signal between the Wiser Hub and the relay.

  2. The relay is working in degraded mode.

  1. Check Hub is online.

  2. Check signal strength.

The relay is flashing green.

Emergency heat is active.

Press the button to cancel the emergency heat function.

TIP: See also LED Indications – Understanding LED status and corresponding corrective actions.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.