DUG_Micro Module Dimmer_WH-08

Manual operation

When the is connected to a mechanical push button, the connected lighting devices can be controlled manually.

  • Short press the mechanical push button to turn on/off the light.

  • Press and hold the mechanical push button to adjust the dimming level of the light.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.