DUG_Micro Module Dimmer_WH-08

Pairing Wireless switch with Micro Module Dimmer (Puck)

To pair the Wireless switch to the Puck, you must put the Wireless switch and the Puck into the pairing mode at the same time.
NOTE:

The pairing mode will be active for about a minute.

  1. Short press the right side of the rocker 5 times in quick succession on the Wireless switch.
    The status LED blinks green.
    WARNING
    HAZARD OF ELECTRIC SHOCK
    • Observe the regulations for working on live parts.
    • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  2. Follow any one of the options to pair Puck :
    • Short press the setup/reset button 5 times in quick succession on the Puck with a screwdriver.
      or
    • Short press the mechanical push-button 5 times in quick succession.
    The status LED blinks green on the Puck LED.
    NOTE: If the Puck is located behind the mechanical push-button, the status LED is not visible.

    The light connected to the Puck blinks for a few times. The status LED stops blinking green on the Wireless switch and the Puck. The Puck can now be controlled by the Wireless switch.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.