DUG_Micro Module Dimmer_WH-08

Selecting a location for the device

Using the Wiser Home app, add the Puck to any room (such as living room, bedroom, kitchen etc).
  1. On the Home screen, tap .
  2. Tap Devices > Micromodule Dimmer > Location (A) to assign the puck to an existing room or a new room (B) and tap Submit.
    TIP: You can also navigate by tapping Controltab, tap > Select the Device > Device Settings.
    NOTE:
    • Tap Remove from Room to remove the device from the existing room.

    • Micromodule Dimmer is the name given to the device by the user. Any name can be assigned when pairing with the Wiser hub.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.