DUG_Micro Module Dimmer_WH-08

Using the device

The Device Control Screen allows you to switch ON/OFF the device and control various settings.

On the Control tab, select the dimmer and the control screen shows the options below.

The Device Control Screen displays the following options:


A

Drag the sliding bar up/down to increase/ decrease the brightness.

B

Tap to manually turn the device ON/OFF.

C

Tap to redirect you to the Schedule screen, where you can create a schedule. For more information, refer to the Setting up a schedule topic.

D

Add to favourites Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide.

E

Tap to control various settings from the Device Settings screen. For more information, refer to the Configuring the device topic.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.