DUG_Micro Module Light Switch_WH-08

LED indication

Pairing the device

User Action

LED Indication

Status

Short press the Setup/Reset button or push-button 3 times.

The LED blinks amber once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED displays green for a few seconds before turning off.

Resetting the device

User Action

LED Indication

Status

Short press the Setup/Reset button or push-button 3 times and hold it down once for > 10 s.

The LED blinks green once, blinks red for a few seconds, then blinks green again and finally turns solid amber.

The device is in reset mode. The device then restarts and LED turns amber indicating that the device is ready for pairing.

Other LED indications

LED Status

Description

Solid Red

The light is turned on.

Solid Green

The device has been already paired to the Hub.

Solid Amber

The device is not paired to the Hub.

Blinking Amber

The device is ready for pairing.

No LED

The light is turned off.

Blinking Green

The Setup/Reset button was pressed 3 times while the device was already paired to the Hub.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.