Pairing the device with the Wiser Hub
- On the Home screen, tap
.
- Tap .
- Tap Scan QR code and allow the Wiser
Home app to access your camera. Then, scan the QR code located on
the device.NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.
If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:
-
(A): Enter the MAC Address and Install Code, then tap Connect. The app will verify if the MAC address and Install code are valid.
-
(B): Tap this option if you are unable to find the MAC address and Install code.
-
- Tap Next and select any one of the
options to add the device:
- Short press the Setup/Reset button 3 times on the puck with a screwdriver and make sure the LED blinks amber.
- Short press the push button 3 times.
NOTE: If the puck is located behind the push button, the status LED is not visible.
Wait for a few seconds until the LED turns green and the app confirms that the device is joined.
NOTE: If the LED is blinking green and red, see the instructions by tapping LED blinking green and red? or refer to the Troubleshooting topic. - Tap Next to enter the name of the
device and assign the device to a new room or an existing room. Then,
tap Submit.
After you pair the device, a success screen appears with the following options:
-
+ Add New Device: Tap to continue pairing more devices.
-
Start Using Your Device: Tap to start using the paired device.
NOTE: The success screen appears only if you are logged in as a Home Owner.The puck is now listed on the Control tab under the All and Room tabs.
-