DUG_Micro Module Shades Control_WH-09

Removing the device from Wiser system

Using the Wiser app, you can remove the Puck from the system.
  1. On the Home screen, tap .
  2. Tap Devices > Shutters > Micromodule Shutter or Shutter slat > Delete (A).
    NOTE:
    • Removing the device will reset the Puck. The LED starts blinking amber indicating that the Puck is ready to pair.

    • If there is a problem while pairing or resetting the Puck, refer to Resetting the device manually.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.