DUG_Micro Module Shades Control_WH-09

Setting the start and end time

Using the Wiser Home app, you can define the start and end time of the seasonal comfort mode.

To set the start and end time of the seasonal comfort mode:
  1. In the Seasonal Comfort Mode set-up page, tap Time.
  2. Select the time when the seasonal comfort mode will BEGIN AT and the time when it will FINISH AT.
    NOTE: You can start and stop the seasonal comfort mode some time before or after the sunrise/sunset.
  3. Tap Set.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.