DUG_Micro Module Shades Control_WH-09

Testing the device

Before using the Puck, manually test the Puck and make sure that it works when connected to the shutter.

WARNING
HAZARD OF ELECTRIC SHOCK
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

To test the Puck:

  1. Short press the test button once.
    The shutter opens/closes gradually.

  2. Press and hold the test button.
    The shutter opens/closes fully.

  3. Record the time for the shutter to fully open/close.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.