Troubleshooting
|
Symptom |
Solution |
|---|---|
|
No shutter movement or uncontrolled shutter movement. |
|
|
The device is not ready to pair after the device is removed from the app. |
Reset to factory default settings, refer to Resetting the device manually |
|
The shutter/blind no longer works manually. |
Press the Test button on the puck to confirm that the shutter/blind is working. If it functions properly, the problem is with the mechanical push button wiring. |
|
The shutter/blind does not open or close completely. |
Check the open/close duration defined on the Device Details screen. If the open/close duration is incorrect, the shutter/blind may stop before reaching the fully open or fully closed position. Adjust the calibration duration as needed. For more information, refer to setting the configure duration. |