DUG_Motion Sensor_WH-07

Resetting the device

You can reset the sensor to factory default manually.
To reset the sensor:
  1. Rotate the sensor counterclockwise to unlock it from the base plate.
  2. Short-press the function key three times (<0.5 s) and then long-press the function key once (>10 s); the LED blinks red after 10 s, then release the function key.
    Upon successful reset of the sensor, the LED stops blinking. The sensor restarts and blinks green for a few seconds.
    NOTE: After reset, the LED turns off to save the battery.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.