DUG_Multiwire Puck Dimmer_WH–05

Configure Connected Switches

You can connect one or two mechanical push-button switches to the dimmer. Each switch can be configured to control the light individually or to activate a moment for switching on/off and dimming up/down.
  1. On the Home screen, tap .
  2. Tap Devices > Micromodule - Dimmer > Configure Connected switches (A).
  3. Select the push button which you want to configure.
    • Push Button 1
    • Push Button 2
    By default, push button 1 is configured with Connected Light Control, and you can configure it to the following options based on your need.
  4. Select any one of the following:
    • Connected Light Control (B)
    • Moment (C)
    NOTE: In the following section, an explanation of the above-mentioned options can be found.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.