DUG_Power_Micromodule_WH-07

About the device

The Wiser Power Micromodule hereinafter referred as module is for switching loads (up to 3000 W resistive) such as a hot water tank or a socket outlet. In combination with the Wiser app, the energy consumption can be measured and the module can be used for load shedding or demand response. Load shedding is used to balance the demand and supply of electricity. Demand response refers to the ability of devices to be automatically controlled or limited by signals sent from your power supplier to your smart meter.
Up to 20 modules can be added in the same system.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.