DUG_Power_Micromodule_WH-07

Creating a moment

To create a moment:
  1. On the Home screen, tap > Moments > .
  2. Enter the name of the moment (A).
  3. Tap Add actions (B) to select the list of devices.
  4. Select the devices (C) you want to set an action and tap Done.
  5. On the Moment creator page, select any one of the following device (D) and set actions.
  6. Tap Off/On as per need and tap Set.
  7. Once all conditions are set, tap Save.
    The saved moment is shown on the Moments tab.
    You can tap on the moment to enable it.
TIP:
  • If you want to see the created moments on the Home screen, go to Home > > Home Screen > Moments. Enable the toggle button to view moments on the Home screen.

  • You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.