DUG_Power_Micromodule_WH-07

Editing an automation

To edit an automation:
  1. On the Home screen, tap > Automation.
  2. Tap the automation you want to edit.
  3. On the Edit automation page, you can:
    • Change the icon.
    • Rename the automation.
    • Change the condition or action.
  4. Remove the Condition or Action by swiping it to the left and tapping the .
  5. To change the order of actions, tap the Then option, and hold an action then drag and drop to the desired position.
  6. Add a new condition or action and then tap Save.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.