DUG_Power_Micromodule_WH-07

Using the device

The Water Heater Control Panel allows you to turn on or off the device and monitor the power consumption.

On the Control tab, tap All devices or a room tab where the Plug is located > Water Heaterto access the control panel.

On the Device Control Screen, you can see the following:

A

Total energy consumption in the session

B

Tap to manually turn the device ON/OFF.

C

Device can be controlled and triggered by a schedule. You can change to any one of the following schedule modes:

  • Manual:

    Device will start when you turn on. If it is already switched on, it will start directly.
    NOTE: By default, the device will be in manual schedule mode.
  • Wiser Home AI: This feature automatically schedule your loads when the cost is the cheapest. Refer to Wiser Home AI.

  • Customised schedule: You can create your own schedule to turn on or off your device. Refer to Creating a schedule topic.

D

You can see the 24 hr schedule for the device based on the electricity rates.

E

You can rename the device or remove the device from the Wiser system, change location, nominal power. Refer to Configuring the device.

F

Add to favourites (F) - Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide..

NOTE:

Similarly you can control and check the current status of Water Heater from Control tab.

  • Tap to turn on/ off the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.