DUG_Wiser Plug_WH-11

Pairing the device with the Wiser Hub

Using the Wiser Home app, pair your Plug with the Wiser Hub to access and control the Plug.
  1. On the Home screen, tap .
  2. Tap Devices > > Appliances > Smart Plug.
    TIP: You can also navigate by tapping Control > > Appliances > Smart Plug.
    TIP: The next screen shows the joining process of the Plug.
  3. Press and hold the ON/OFF button for 2 seconds on the Plug until the LED flashes blue.
    The Plug is now successfully joined.
  4. Tap (A) to select an icon suitable for your load, and tap Save.
    NOTE: Electric plug icon is assigned by default.
  5. Tap (B) to assign a name.
  6. Tap Next to assign the Plug to an existing room or a new room.
  7. Tap Submit.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    Now, you can see the newly added device on the Control tab under the All and Room tabs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.