DUG_Smoke alarm DC_WH-05

Setting the device location

You can add your device to any room (such as bedroom, living room, dining room etc.).
  1. On the Home screen, tap .
  2. Tap Devices, select the device from the list for which you wish to change the location.
  3. Tap Location to open setup screen.
  4. On the Device Setup screen, you can enter New room name (A) or select an existing room from the list (B).
    TIP: If the device is already assigned, you can remove it from the existing room. Tap Remove from Room (C).
  5. Once changes are done, tap Submit (D).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.