DUG_Smoke alarm DC_WH-05

Using the device

The Control Panel of the smoke alarm allows you to view the current state of the smoke alarm and allow you to access the history and settings.
  1. On the Control tab, tap All devices or a room tab where the smoke alarm is located.

  2. On the Smoke Alarm control panel page, you can see the following:

    • Current state of the smoke alarm (A)

    • History (B)

      NOTE: The history page gives information about the smoke alarm (date, time, and type of alarm detected, for more information, refer to Checking the device history).

    • Device settings (C)

      NOTE: The smoke alarm setting page gives information about setting the LED brightness of the smoke alarm, for more information, refer to LED brightness settings.

    • Add to favourites (D)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.