DUG_Smoke alarm DC_WH-05

Identifying the device

Using the Wiser Home app, identify the device among the smoke alarms available in a home.
  1. On the Home screen, tap .
  2. Tap Devices > > Identify (A).
    NOTE: The LED on the smoke alarm may take up to 60 minutes to blink and identify. This delay depends on when the smoke alarm communicates with the hub during its regular.
  3. Tap OK to finish identifying the device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.