Path

This tab displays a one-line subway diagram of the circuit. The following symbols help you orient yourself within the diagram:

Symbol

Description

The start of the circuit

The origin of the trace

The end of the circuit

A patch location

A splice

The diagram also shows ports through which the circuit passes, fibers and their glass lengths, as well as trays at splice cases.

The Circuit Path diagram contains additional information and navigation tools:

  • Click the name of a fiber feature to jump to that feature’s detailed connection page in Wavepoint.

  • Click the Zoom  button to navigate to that feature in the map.

  • Click the Flip   button to reverse the start and end points of the one-line diagram.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.