DOCA0265EN-08

Access Management Per Access Path

General Description

Data on MicroLogic Active control units can be accessed:

  • From the MicroLogic Active HMI (PIN code protected)

  • On a device connected to the MicroLogic Active USB-C port (password protected):

  • On remote controllers through the ULP modules of the IMU system

  • On a smartphone running EcoStruxure Power Device app through NFC connection

  • On Panel Server webpages and on servers or remote controllers connected to Panel Server, through Zigbee wireless communication (MicroLogic Active AP/EP control unit only)

The following table describes the functions which can be accessed via each access path, and the required protection mechanisms (if any).

Function

Description

Access path

HMI

USB port

IMU

Zigbee

NFC

Monitoring

Read settings, measurements, and data

✔

-

✔

✔

✔

Settings

Set MicroLogic Active control unit settings

✔ (1)

✔ (2)

✔ (4)

-

-

Reset counters

Reset minimum and maximum values

✔

-

✔

-

-

Test

Send test commands

✔ (1)

-

-

-

-

Firmware update

Update firmware to the latest version

-

✔ (2)

-

-

-

Operation

Send commands to open and close the circuit breaker

-

-

✔ (3)

-

-

MicroLogic Active replacement

Set the settings of a replacement MicroLogic Active control unit

✔ (1)

-

-

-

-

✔ Access allowed without restriction

✔ (1) Access protected by PIN code

✔ (2) Access protected by USB password

✔ (3) Access only allowed in Auto Remote control mode

✔ (4) Access only allowed when the Remote Setting parameter is set to ON

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.